I have a question. Someone already use the am335x and KSZ9031?
I have a custom board, this board is based in Starter Kit and KSZ9031RNX Evaluation Board.
And in my case the status of the LED1 toggle and LED2 your state is high, have signals in pin RX, but TX enable and pin TX are in down. The kernel recognizes the phy:
[ 65.114071] net eth0: CPSW phy found : id is : 0x7c0f1
But I when do ifconfig, don't have RX or TX, 0 bytes
root@am335x-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr BC:6A:29:99:F3:58
inet addr:192.168.1.221 Bcast:192.168.1.255 Mask:255.255.255.0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
what can be?
thanks