I have a TMDXEVM3588, (Base Board, Daughter Board, LCD and Wifi).
I have J18 running I2C I/O Expansion, but it's not fast enough for what I need.
I'd like to use GPIO, however it seems that there are no connectors available which provide GPIO when
the board is configured as above (i.e. all the pins are being used by something)
What's the recommended way of accessing GPIO on the hardware? Do I need to put something between the boards?