Hi all,
We are planning to use AM3352 with eMMC as boot as well as storage media.
I can see from Wiki pages that common used size is 2 GB.
Can anyone confirm the maximum possible size of eMMC for AM3352 ?
Thanks in advance !
Regards,
Sweta
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
We are planning to use AM3352 with eMMC as boot as well as storage media.
I can see from Wiki pages that common used size is 2 GB.
Can anyone confirm the maximum possible size of eMMC for AM3352 ?
Thanks in advance !
Regards,
Sweta
Just wanted to say this was helpful in reminding me that MMC1 needs to be used if the MMC is larger than 4GB, Thanks.
If they are eMMC v4.41 spec compliant then they could be used without any issues.
Hello Rogerio,
according to the TRM the MMC0 cannot boot devices greater than 4GByte. Does the boot ROM code set the Bit 30 in the CMD1 when the device is High Capacity? (Reading the eMMC OCR register content like 0xC0FF8080). If not, I can't use Micron eMMC devices because they expect it. But Kingston devices boot without sending this Bit as command argument ("host is capable of handling sector type of addressing"). Currently I have a 8GByte Micron eMMC connected to MMC0 which does not boot.
Thanks in advance,
Stephan