Hello,
The TRM (i) shos that the AM335x support booting from a 2k + 64 NAND:
Support for large page size (2048 bytes + 64 spare bytes) or very large page size 4096 bytes + 128 /
218 spare bytes)
Can it also boot form a NAND device that has 2k pages and 128 spare bytes?
Will I need to write the ECC bits with a stride or at the beginning (after bb marker)?
Will the ROM code expect BCH8?
This is the NAND: <http://www.spansion.com/Support/Datasheets/S34ML01G2_04G2.pdf>
(S34ML04G2 in x8)
Regards,
Lo2