Hello,
I have the same problem that this post : http://e2e.ti.com/support/arm/sitara_arm/f/791/p/238902/1052093.aspx#1052093
But the proposed solution isn't effective in my case.
Before doing the change, the SUBARCTIC peripheral connect and disconnect every 10 sec.
When the SUBARCTIC disconnect, my serial port write CCCCCCC, then it connects back, and I stop receiving anything.
I'm on W7, I've made the NDIS change with the SUBARCTIC peripheral but my serial port still doesn't work:
- I boot on a SD card with a MLO and a bootrom
- I link my laptop and the SSK by the microUSB
- I setup my realterm to a serial connection
I only receive CCCC when I reset the board (the time that the SUBARCTIC reconnect)
I've tried this on 2 computers, and on Linux. Linux detect the SUBARCTIC has a Texas Instrument Network.
I don't get it...