Hello TI community,
i'm trying to interface an audio adc (wolfson wm8782) with the Beagle Black (running Ubuntu 13.10 kernel, 3.8.13-bone39).
My problem is that i cant make the kernel register the "soundcard", i'm struggling with the files davinci-evm.c and with the codec driver wm8782.c (please see below for the code). I don't know if this is the right way or there is an easy way using device tree overlays...
I'll appreciate any help!
Thanks!
davinci-evm.c
/* * ASoC Driver. * * This program is free software; you can redistribute it and/or * modify it under the terms of the GNU General Public License * version 2 as published by the Free Software Foundation. * * This program is distributed in the hope that it will be useful, but * WITHOUT ANY WARRANTY; without even the implied warranty of * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU * General Public License for more details. */ #include <linux/module.h> #include <linux/platform_device.h> #include <sound/core.h> #include <sound/pcm.h> #include <sound/pcm_params.h> #include <sound/soc.h> #include <sound/jack.h> static int evm_wm8782_init(struct snd_soc_pcm_runtime *rtd) { return 0; } static int evm_wm8782_hw_params(struct snd_pcm_substream *substream, struct snd_pcm_hw_params *params) { struct snd_soc_pcm_runtime *rtd = substream->private_data; struct snd_soc_dai *cpu_dai = rtd->cpu_dai; /*return snd_soc_dai_set_bclk_ratio(cpu_dai, 32*2);*/ return 0; } /* machine stream operations */ static struct snd_soc_ops evm_wm8782_ops = { .hw_params = evm_wm8782_hw_params, }; static struct snd_soc_dai_link evm_wm8782_dai[] = { { .name = "wm8782 board", .stream_name = "wm8782 board", .cpu_dai_name = "davinci-mcasp.0", .codec_dai_name = "wm8782-hifi", .platform_name = "davinci-pcm-audio", .codec_name = "wm8782-codec.3-001b", .dai_fmt = SND_SOC_DAIFMT_I2S | SND_SOC_DAIFMT_NB_NF | SND_SOC_DAIFMT_CBS_CFS, .ops = &evm_wm8782_ops, .init = evm_wm8782_init, }, }; /* audio machine driver */ static struct snd_soc_card snd_wm8782_adc = { .name = "snd_wm8782_adc", .dai_link = evm_wm8782_dai, .num_links = ARRAY_SIZE(evm_wm8782_dai), }; static int snd_wm8782_probe(struct platform_device *pdev) { int ret = 0; snd_wm8782_adc.dev = &pdev->dev; ret = snd_soc_register_card(&snd_wm8782_adc); if (ret) dev_err(&pdev->dev, "snd_soc_register_card() failed: %d\n", ret); return ret; } static int snd_wm8782_remove(struct platform_device *pdev) { return snd_soc_unregister_card(&snd_wm8782_adc); } static struct platform_driver snd_wm8782_driver = { .driver = { .name = "snd-wm8782-adc", .owner = THIS_MODULE, }, .probe = snd_wm8782_probe, .remove = snd_wm8782_remove, }; module_platform_driver(snd_wm8782_driver); MODULE_AUTHOR("E.E.R"); MODULE_DESCRIPTION("ASoC Driver for pcm1803 ADC"); MODULE_LICENSE("GPL v2");