Hi,
I am sorry for posting TPS65910 question here, I will ask the same in the PMU forum
but I would like to know if there are any suggestions in this forum also.
Our customer board has TPS65910AA1 as PMIC IC to power up AM3352.
But unfortunately the TPS65910AA1 is not working (so AM3352 is not working).
There is no output from the TPS65910 IC even after applying power.
Seems like either the IC is dead or the circuit is wrong.
All the connections are done as per the TI's reference boards Schematics.
PWRHOLD and PWRON pins are connected as below.
PWRHOLD -> Connected to an external 3.3V power to keep it High
PWRON -> As we don't need the push button, PWRON pin is left floating
And below are the results of few test points after applying power to TPS65910.
INT1 -> 0V
SLEEP -> 0V
PWRON -> 5V
BOOT0 -> 0V
BOOT1 -> 1V
PWRHOLD -> 3.3V
Just in case I am attaching the our schematics.
Please let me know what else should be tested to analyse the problem
and is it ok to leave PWRON pin floating if the push button is not necessary?
Regards
Prad