Hello,
In the reference manual the following is written:
• MMC0 supports booting from the MMC/SD card cage and also supports booting from
eMMC/eSD/managed NAND memory devices with less than 4GB capacity.
• MMC1 supports booting from eMMC/eSD/managed NAND memory device with 4GB capacity or
greater.
Now I like to use and 8Gb or 16GB sd card to boot from MMC0, can this be possible with maybe two partitions?
Kind regards
Patrick