I would like to be able to boot from the USB0(ROM loader) into U-Boot then boot from a USB drive on USB1 is this possible? This would only be until I get the eMMC loaded with the proper files.
Another solution could be the DFU but it appears to not be in the latest u-boot in sdk 7.0.
Also porting u-boot for a am335x is in note straight forward and something a simple as moving I2C from 0 to 1 is quite difficult.
Any tips would be great thanks