Hi,
I prepare to use AM3359 for data transmission over serial line. The system is Linux based and the line must be seen for Linux as an Ethernet device for compatibility reasons. Please tell if it is possible to take ready Ethernet frames from MAC module for processing in PRU and put received frames there?
If I understood correctly, the third parties PRUSS firmware (EtherCAT, Profinet etc.) takes payload from shared memory and replaces the ordinary MAC module functionality, assembling Ethernet frame and driving MII outputs?