Hi,
I'm using AM3359 on my custom device (based on TMDXICE3359)
Do I re-design my device circuit in order to use AM335x silicon v2?
Is there any change of pin assignment or something?
Thank you.
Teyun.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm using AM3359 on my custom device (based on TMDXICE3359)
Do I re-design my device circuit in order to use AM335x silicon v2?
Is there any change of pin assignment or something?
Thank you.
Teyun.
I recommend you read the AM335x Silicon Errata. This document describes a few differences. For example, Advisory 1.0.6 describes the polarity change of the EXTINTn input.
Another example, is the difference between Usage Note 3.1.4 and 3.1.6. The rmii2_crs_dv signal was added as another pin multiplexing option to Mode2 of the gpmc_csn3 pin and Mode3 of the gpmc_a9 pin.
Note: You should be using the pin mux tool to verify AM335x pin assignments. Make sure you select the correct silicon revision when you start the pin mux tool.
The AM335x TRM also has a section discussing silicon revision differences.
Regards,
Paul