Hi
We are working on a customboard based on AM335x Starter Kit EVM with AM3352 SoC and currently porting U-Boot on our board. We already configured U-Boot SPL to run on our board (and also tuned and test DDR3 using CCS), we only needed NAND, DDR3 and serial config files for the U-Boot SPL to run on our board (using UART0 Boot). The U-Boot SPL successfully run Loaded u-boot.img through UART YMODEM but after that nothing happened and i hangs. I connect our board through JTAG and use CCS to check the DDR is working properly by going into Memory watch window and write some data on the DDR3 address and it is working, I check also PC register and found out that it stop at address 0x249CB3B8.
My question is after U-Boot-SPL loaded the u-boot.img through YMODEM should it jump into 0x80800000 location where the u-boot.img is loaded? By the way we are using am335x-evm-sdk-src-07.00.00.00.
Any clue on this? We are stuck on this problem for weeks now.