So I'm trying to get a starterkit evaluation board up and running with the SDK 7.0.
I attached a picture on the board just to make sure I in fact is running on a starterkit. I can't see that name anywhere on the board. but the label has it at revision 1.2b.
I have downloaded ti-sdk-am335x-evm-07.00.00.00-Linux-x86-Install.bin and installed it. created a sdcard from that and booted it up. it starts.
But here is the thing. when I do
echo mem >/sys/power/state. it just hangs ? should this not work ? where have I gone wrong ??
I tried the original prebuilt images and the kernel and device tree built when doing make by loading them from tftp server. I'm using the device tree named am335x-evmsk.dtb. and the kernel image from ./board-support/linux-3.12.10-ti2013.12.01/arch/arm/boot/zImage.
So how do I get suspend to work on this board with sdk 7.0.