i use TI Linux SDK6.0
1.how to run QT application program in TI base filesystem (arago-base-tisdk-image-am335x-evm)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
i use TI Linux SDK6.0
1.how to run QT application program in TI base filesystem (arago-base-tisdk-image-am335x-evm)
Hi Jelliott
The arago-base-tisdk-image-am335x-evm.tar.gz is a barebones filesystem. It includes things like busybox and other packages but doesn't include alot of larger libraries like Qt, Gstreamer etc.. Its a good starting point for customers who want a minimal filesystem that can boot that they can later install additional software on top of.
Tisdk-rootfs-image-am335x-evm.tar.gz is our full blown filesystem that includes every package we generally support. Qt,Gstreamer, SGX, etc.. This is also useful for customers who want to create quick demos or prototyping something using a filesystem that has the majority of the software that they may need already prebuilt.
Execution results are as follows:
1.arago-base-tisdk-image-am335x-evm.tar.gz
root@am335x-evm:/media/mmcblk0p1# ./helloworld
./helloworld: error while loading shared libraries: libQtGuiE.so.4: cannot open
shared object file: No such file or directory
2.Tisdk-rootfs-image-am335x-evm.tar.gz
I used Tisdk-rootfs-image-am335x-evm.tar.gz file system to test QT no problem