The DM3730CUS datasheet per the "Other Balls" specification says that pins should be keep with 0.3V of the rails. This is difficult to do with a DRAM bus. The JESD209B specification for mDDR says that overshoot/undershoot can be 0.5V as long as the integrated area of the overshoot/undershoot is less that 3V-ns. This also appears to be near what Micron states (1V for <3ns). So are the DRAM controller I/O on the DM3730 compliant to the JEDEC specification? I'm seeing about 360mV of undershoot and no overshoot.