Hi,
I am working with ddr2. Using am335x. I have done with the configuration and initialization codes for interfacing ddr2 with emif controller on am335x.
In the ddr2 data sheet, there is some initialiation sequence. How to do that?
1. Apply power and attempt to maintain CKE below 0.2 × VDDQ and ODT*1 at a LOW state (all other
inputs may be undefined.) Either one of the following sequence is required for Power-up.
A. The VDD voltage ramp time must be no greater than 200 mS from when VDD ramps from 300
mV to VDD min; and during the VDD voltage ramp, |VDD -VDDQ| ≤ 0.3 volts.
VDD, VDDL and VDDQ are driven from a single power converter output
VTT is limited to 0.95V max
VREF
*2 tracks VDDQ/2
VDDQ ≥ VREF must be met at all times
B. Voltage levels at I/Os and outputs must be less than VDDQ during voltage ramp time to avoid
DRAM latch-up. During the ramping of the supply voltages, VDD ≥ VDDL ≥ VDDQ must be
maintained and is applicable to both AC and DC levels until the ramping of the supply voltages
is complete.
Apply VDD/VDDL
*3 before or at the same time as VDDQ
Apply VDDQ
*4 before or at the same time as VTT
VREF
*2 tracks VDDQ/2
VDDQ ≥ VREF must be met at all times.
2. Start Clock and maintain stable condition for 200 μS (min.).
3. After stable power and clock (CLK,CLK ), apply NOP or Deselect and take CKE HIGH.
4. Wait minimum of 400 nS then issue precharge all command. NOP or Deselect applied during 400
nS period.
5. Issue an EMRS command to EMR (2). (To issue EMRS command to EMR (2), provide LOW to
BA0, HIGH to BA1, LOW to BA2.)
6. Issue an EMRS command to EMR (3). (To issue EMRS command to EMR (3), provide HIGH to
BA0 and BA1, LOW to BA2.)
7. Issue EMRS to enable DLL. (To issue DLL Enable command, provide LOW to A0, HIGH to BA0
and LOW to BA1-BA2 and A13. And A9=A8=A7=LOW must be used when issuing this command.)
8. Issue a Mode Register Set command for DLL reset. (To issue DLL Reset command, provide HIGH
to A8 and LOW to BA0-BA2 and A13.)
9. Issue a precharge all command.
10. Issue 2 or more Auto Refresh commands.
11. Issue a MRS command with LOW to A8 to initialize device operation. (i.e. to program operating
parameters without resetting the DLL.)
12. At least 200 clocks after step 8, execute OCD Calibration (Off Chip Driver impedance adjustment).
If OCD calibration is not used, EMRS to EMR (1) to set OCD Calibration Default
(A9=A8=A7=HIGH) followed by EMRS to EMR (1) to exit OCD Calibration Mode
(A9=A8=A7=LOW) must be issued with other operating parameters of EMR(1).
13. The DDR2 SDRAM is now ready for normal operation.
Regards,
J Sudha