Hi There, I am writing UART2 & UART 4 driver from scrach as it is not available from starterware. I am reading
"AM335x Sitara™ Processors, Technical Reference Manual" It is mention register name but did not find the actual addrees. When i look at the starterware, it is define
#define SOC_PRCM_REGS (0x44E00000)
When i look at the document, it say
1. Initiate a software reset: Set the UARTi.UART_SYSC[1] SOFTRESET bit to 1
Q1. How to get the address(memory map) of the register? Example
UART0_BASE_REGISTER 0x480000, some think like that