Current build : 3.12.10-ti2013.12.01
I have an application source which I cannot cross compile. I would like to natively compile the source on the EVM. However, "make" is not available with the present build.
Is there a opkg package that i can install to add native compile ?
If not, is there a way to add "make" package during targetFS build using create SD card script ?
If not, is there a way to add/build open embedded recipe with make using "http://processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Getting_Started_with_Openembedded" ?
Btw, getting started with open embedded lab is broken at these places(its not a git problem)
cd <oe-dir>/sources git clone git://gitorious.org/sitara-bootcamp/meta-custom.git -b amsdk-06.00.00.00
or
git clone git://gitorious.org/sitara-bootcamp/meta-custom.git -b amsdk-07.00.00.00
or
git clone git://gitorious.org/sitara-bootcamp/meta-custom.git -b amsdk-07.01.00.00
I had also tried
Arago build environment setup(http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment) is broken because of a file fetch from an non-existing link from ti git
at this step
MACHINE=am335x-evm bitbake core-image-minimal
because of an non-existing fetch link.
I want to natively compile a program either by installing a package or by building a OE based build. I would greatly appreciate help for this.