Hi Sir:
I use AM3358 on my custom board.
My u-boot is u-boot-2013.01.01-psp06.00.00.00
When I use nand flash to boot up our system, u-boot hang up.
Below is the log.
U-Boot SPL 2013.01.01 (Aug 01 2014 - 13:34:04)
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Peripheral mode controller at 47401000 using PIO, IRQ 0
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
USB Host mode controller at 47401800 using PIO, IRQ 0
Is there something that I should take attention about flashing image from SD to nand?
My sysboot setting is 00100b and my system works when boot up from SD.
Please give me your suggestion!
Best regards,
Marcus