Hi all,
I want to check whether the VPFE port of the AM437x can work in master mode or not?
That is, the VD/HD should be in out mode when the AM437x VPFE work as a master.
And I have checked the TRM Table 14-5. Summary of VPFE Signal Pins and Common Input Devices, the VD/HD mode is as below:
For the RAW mode, the VD/HD mode is as below
For the Ycbcr mode, the VD/HD mode is as below:
So even the table 14-5 shows that the VD/HD can support the Input and out mode, but the description in each mode shows it support the input mode only.
Then which one is correct?
Thanks!
Yaoming