Hi,
I am working on a prototype board that is based on the AM335x but with AM3358 StarterKit SDRAM (don't ask why..). I am currently using WindRiver Workbench (as the target OS is VxWorks). Needless to say the DDR3 doesn't work and the only way I can see to obtain the correct register values is to run the software levelling algorithm on CCS.
So, if we buy CCS and a XDS200 probe (the proto has a 20-pin jtag facility), and all goes well, should this be sufficient to determine these regiseter values?
Of course I'd need a modified AM3358 StarterKit GEL file and the DDR3_slave_ratio_search_auto.out file.
Also, am I correct in saying the DDR3_slave_ratio_search_auto.out file is run by CCS and not on-board?
Thanks in advance,
David.