After building a few images with Yocto I decided to try and use just OE Core and meta-ti. After building core-image-base I was unable to boot from the same SD card I have been using. I notice the version of uboot is much newer in meta-ti. When I hold the user button my BeagleBone Black to boot off the SD card I get the following on the console:
U-Boot SPL 2014.07 (Aug 29 2014 - 13:15:48)
MMC: block number 0x100 exceeds max(0x0)
MMC: block number 0x200 exceeds max(0x0)
*** Error - No Valid Environment Area found
Using default environment
MMC: block number 0x1 exceeds max(0x0)
** Can't read partition table on 0:0 **
** Partition 1 not valid on device 0 **
spl_register_fat_device: fat register err - -1
### ERROR ### Please RESET the board ###
The card partition is as follows:
Disk /dev/mmcblk0: 31.7 GB, 31691112448 bytes
4 heads, 16 sectors/track, 967136 cylinders, total 61896704 sectors
Units = sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x00000000
Device Boot Start End Blocks Id System
/dev/mmcblk0p1 * 63 144584 72261 c W95 FAT32 (LBA)
/dev/mmcblk0p2 147456 7127039 3489792 83 Linux
My boot partition has MLO and u-boot.img. This was enough with Yocto but using this new u-boot do I need more there? I am not using a uEnv.txt file.