I am currently using the AM3352BZCZ80 for a product the technical reference manual states that the MVR register should be formatted as such:
Bits 15-8 - reserved, bits 7-4 Major Rev and Bits 3-0 Minor Rev, When I read this register I get a 0x2603, making it version 0 3. This seams to be what I have seen referred as to as the "OMAP4" type MVR version. which would make it 6 3 which make more sense can someone confirm A. if the documentation for this register is correct and B what the MVR should be for this UART on this part.