Hi,
We are using VAR-SOM-OM37 module and want to use up to eight external displays with a mcp2210 chip from Mikrochip on USB host via an USB hub. My problem is, that if more than one device is plugged, (i guess) the driver seems to be too slow to handle the write process to the displays. If i plug in the hub on the OTG port, then musb_hdrc is loaded and all displays work fine, but it could be faster.
We can't upgrade from kernel 2.6.32 by now, but is there any way to speed up the USB host side?
Kind regards,
Silke