I am designing system with two SItara AM335x processors ( most likely AM3352 )
My original idea was to use separate TPS65217C chips and just combine PGOOD from them - to avoid non-sequencial power of cpu's ( which do have interconnections) . This plus slaved external 3.3V dc/dc converter ( I need quite much for peripherials - almost 2A )
But is there a better way ? Is there a chip which could handle both CPU at once (TPS65217x does not hint it could be used like that) ?
I will not be using any sleep mode - basically full power from the start, no sleep modes.