This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Which version of the SDK are you using?
Try to flash the mtd partitions from U-Boot as I have explained here: http://e2e.ti.com/support/arm/sitara_arm/f/791/p/268305/949397.aspx#949397
There are also explanations about the needed calculations. Verify that yours are correct.
Best regards,
Miroslav
The U-Boot from the SDK you are using has the following command:
ext2load- load binary file from a Ext2 filesystem
Type "help ext2load" for more information.
Best regards,
Miroslav
There is no enough space available to store ubi.img in mmc0. My ubi.img file is 342 MB.i also tried using
fatload mmc 1 0x820000000 ubi.img ,but it is not coming out of that command.
Please suggest me in this regard.
Regards,
Ajith
Hi, There is no space to load ubi.img in the mmc0. ubi.img is stored in mmc1(rootfs partition of SD card). From u-boot terminal I tried ext2load mmc 0:1 0x82000000 /ubi.img O/p: Failed to mount ext2 filesystem... ** Unrecognized filesystem type ** Please teach me how to attach and mount ubi.img. Regards,
Ajith
How is your rootfs partition formatted? Is it ext2 or ext3 or ext4? If it is ext4, the ext2load command won't work. To work around this issue, either format the partition as ext2 or enable ext4 support in U-Boot. Read more about it here: http://lxr.missinglinkelectronics.com/#uboot/doc/README.ext4
Best regards,
Miroslav