Dear all,
I developped two boards,formlly the first board use CPU AM3352,(DDR3)512M sansung K4B4G1646B 1066MHZ, U-boot can run normally,and linux kernel can also boot up ok.
But now,the second board I only changed the DDR3,using K4B4G1646D-MCK0 1600MHZ,except it nothing has been modified on board.Every time ,u-boot run stopping on at starting kernel .
I find that click on U-boot cmd:DCache on,the board is dump .but ICache on is ok.
Note:the two board DDR3 cfg are ok,I sure that I make it according to SW LEVELing ,use CCS tool ,make DDR test,they are both ok.
So I wonder that what is wrong?Who can help me?thanks a lot!