Hello,
I've been testing our BeagleBoneBlack boards with the 3.12 SDK 7 kernel. Everything seems to be working fine except that the BBB sometimes reboots unexpectedly (this is happening about once per day on multiple boards) at random times throughout the day. I have not seen this happen with the 3.8.13 kernel (using the exact same boards with exact same power supplies).
This is occurring both on version A5B boards and version B boards (I haven't tested any other versions).
When the board reboots the system date/time gets reset. This leads me to believe that the RTC is stopping somehow. With the 3.8.13 kernel the system date/time is only lost if the board is completely unpowered; the time is kept through software reboot, reset button reboot, and watchdog reboot.
I've tried changing power supplies but the issue remains.
Is anyone else having this issue? Any ideas as to what might be causing this?
Thanks!