Hi,
We use the pre-built image from TI for our custom beaglebone black board which is integrated with WL8 wifi/bluetooth cape.
We know that there is a limitation that WL8 cape uses the same MMC as the eMMC for the BBB ,once you apply the device tree patch (or use the pre-built images) you can only use the uSD card of the BBB and the eMMC is disabled.
Therefore, We made hardware changes and use different MMC interfaces for WL8 cape( mmc2 ), on board eMMC ( mmc1 ) and uSD card ( mmc0 ). But it requires a pinmux change in the device tree. My questions are as follows:
1. where can I find the DT source file--am335x-boneblack.dts that was used to compile to the am335x-boneblack.dtb file in the pre-built image?
2. After making the pinmux changes in the .dts file, how to recompile the kernel and the device tree source using the following commands.
make omap2plus_defconfig make zImage dtbs make modules make modules_install INSTALL_MOD_PATH=<rootfs location>
If anyone could answer my questions, I would really appreciate it. Thanks.
Shu