Hi,
I am a beginner with the am3359 processor , so after I have installed the CCS 5.5 I have tried to build the project uartecho example and I have the following error messages :
- 3 message :
"C:\ti\am335x_sysbios_ind_sdk_1.1.0.5\sdk/os_drivers/lib/sys_bios_driver.lib
<osdrv_uart.obj>" has a Tag_PCS_config attribute value of "1" that is
different than one previously seen ("0"); combining incompatible files
moreover , every building operation takes (in my opinion) too much time showing the message :
- "C:\ti\ccsv5\tools\compiler\arm_5.1.1\lib\rtsv7A8_A_le_n_v3_eabi.lib" for
the first time, so it must be built. This may take a few minutes.
could TI help me with these problems.
I don't whether I have written all the information needed.....
thanks