Hello,
I have encountered PRU broken issue.
In our 3 target boards, AM3356 ZCZ package [R12] pin is broken for some reason.
And, system block is like below.
[R12] pin is used as DIO output (pr1_pru0_pru_r30_15).
AM3356's PRU DIO output[R12] ----> Resistor 330ohm ----> other device(5V power).
Phenomenon:
- When u-boot is booted up and configure the pinmux as PRU, the [R12] pin broke.
After that,
- After reset, [R12] drives Low(It is same as datasheet spec). Then, [R12] pin drives high when pinmux is set as PRU.
I am assuming that it does Not I/O broken, it might be broken of internal of PRU.
I would like to find any wrong in our system.
Do you have any idea for debugging?
Or, can you provide me equivalent circuit or hint of PRU?
If you need any other informations, please let me know.
I am appreciate any trivial informations.
Best regards, RY