Hi,
I am trying to connect and run on an ICE V2 and having connection problems. I have set up Target config file for the XDS100V2USB connection and am connecting to just the A8 and using the V2 GEL file from the SDK. Most of the time when I connect I get Error -1266 which is "Device is held in Reset".
The problem occurs most of the time but I've had 30 minutes of debugging where worked ok,loaded ran and breakpoints just as it should and then it stopped working for no particular reason.
I have also exactly followed the "Launching and Debugging Application in CCS" in the Getting Started guide and had the same problem.
Note: This is all done in Windows 7 and CCS5.5.
--jim schimpf