We have an AM3352 question about the CPU clock speed. We are using the 800MHz speed grade which we plan to boot at that rate and then switch down to 300MHz afterwards. We came across some info (see the URL in the email below) that says that OPP50 mode disables Ethernet and DDR3 support. We were wondering:
- Does setting the CPU to OPP50 inherently set the CPU clock to 300MHz?
- Does setting the CPU to 300MHz inherently set the CPU to OPP50?
- If the above two things are not the same, how do you set the OPP mode? We have been using the cpufreq-info command in both Angstrom and Arago Linux to view and adjust the clock frequency. Can this command be used to set the OPP mode too?
- Does the OPP mode affect the RAM speed too? Or does the RAM always run at the same speed from boot onward?
http://www.ti.com/product/AM3358/datasheet/peripheral_information_and_timings#SPRS7174426