The installer for the PRU pru-addon-v1.0-Linux-x86-Install.bin gets to the Installation Directory screen and will go no further. It gives me the warning "Error: Directory does not exist" even though the directory does exist. I am selecting the directory (with the file chooser dialog) where I have installed the SDK v7.0 for AM335x. Clearly the directory exists, but the installer doesn't think so.
How do I get past this?
I have tried allowing it to install into the default directory that the dialog is suggesting but that directory doesn't exist either. I manually created it and still the installer thinks it does not exist.