Hi all,
My customer is designing a control board using AM335x and
the board connects USB interface as device/peripheral to host PC.
He try to insert an isolator between USB terminals to USB connector pins.
However AM335x_Schematic_Checklist describes as follows.
Typical connections for a USB peripheral:
-USBx_DP and USBx_DM are connected directly to the USB connector
-USBx_VBUS should be connected directly to the VBUS pin on the USB connector
processors.wiki.ti.com/.../AM335x_Schematic_Checklist
Q1: Is this meant that he should not use an isolator?
Q2: If he can use an isolator, Vbus of an isolator can be supplied 3.3V
from PMIC for AM335x; upstream side, or not?
Best regards,
Kanae