hi all
when i write a 32-bit data and then read it,the lower 16-bit of data is a radom data(the high 16bit is correct).
The board is my custom,the DDR PLL CLOCKOUT is on 400MHz.the sdram chip is MT-ddr3-1600.
I check my emif4d register accoring to the sdram-datasheet timing parameters.and config the PHY register following the TI's wiki,
but the scene still exists.
Is there some register about this,like the burst operation?
thanks advnce.