Hey there,
we are working with the TMDXICE3359 and the Full EtherCAT Slave Stack Code.
We want to expend a data object from the object directiionary.
The sDIInputs should be an array of 37 entries instead of only one.
So we have to adapt the object on code implementation and the esi file.
Is it correct anyway?
The next would be to load the new ESI file to (emulated) eeprom of the AM3359, i guess.
But we cand figure out how to do.
The description given by this link doesn't make sense:
processors.wiki.ti.com/.../AM335x_SYSBIOS_Industrial_SDK_01.00.00.04_User_Guide
We want to create a header file from the xml file.
Kind regards Hendrik