Hi community member,
Would you please provide advice for my problem?
[Problem]
Now my customer would like to use the LCD panel which it is not on EVM for their application. Thus, they modified the driver code (drivers/video/da8xx-fb.c ) of linux such as below.
***************************
[4] = {
.name = "Custom",
.width = 800,
.height = 480,
.hfp = 15,
.hbp = 15,
.hsw = 30,
.vfp = 2,
.vbp = 2,
.vsw = 6,
.pxl_clk = 37100000,
.invert_pxl_clk = 0,
},
*******************************
And they modified the "lcd_init" in "board-am335x_evm.c" in order to read this settings. However, the pxl_clk was 42MHz even though they have set the 37.1MHz.
Where should they modify the code in order to generate the expected clock for pxl_clk?
**************
SDK Version: 6.0
Device : AM3354B
***************
If you have any questions and necessary information, please let me know.
Best regards.
Kaka