Does anyone know of any sample code or if this is possible?
Thanks
Mark
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Garrett,
Can you be more specific?
I had already build the PDK, per those instructions. Deep under "C:\ti\pdk_am335x_1_0_7\packages\ti\transport\ndk\nimu" there is a lib folder, am335x, a8, releaase with a file "ti.transport.ndk.nimu.aa8fg" ... which appears to be a library to link to. I included the file in my project, and have the exact same error.
I can't add the library by name to the linker, the linker is complaining that it can't find the file, despite the full name being set, and the full path being set.
So clearly this is not a library that resolves the missing external.
I then used CCS to try to do an "Import" of CCS projects. I navigate to that folder, and CCS shows an empty box of "projects to import". I even backed up a few direcotries, in the hopes that it can find some example projects anywhere in that tree. Nothing.
So clearly, this isn't a CCS project to import.
I am still left with :
undefined first referenced symbol in file --------- ---------------- NIMUDeviceTable C:\ti\ndk_2_25_01_11\packages\ti\ndk\stack\lib\stk6.aea8fnv<nimu.oea8fnv> error #10234-D: unresolved symbols remain
Any other suggestions?
-CSW
Chris,
You should not need re-build PDK library, instead, you need to follow the wiki section "PDK Example and Test Project Creation"
to create the sample project 'NIMU_BasicExample_bbbAM335x_armExampleproject' which will be under pdk_am335x_1_0_x\packages\MyExampleProjects\ and can be imported to CCS.
see main_bbbAM335x.c for NIMUDeeviceTable,
#define MAX_TABLE_ENTRIES 3
NIMU_DEVICE_TABLE_ENTRY NIMUDeviceTable[MAX_TABLE_ENTRIES];
The NIMUDeviceTable will be referenced by ndk_x/packages/ti/ndk/stack/nimu/nimu.c.
The thread is quite old and titled 'AM437x', can we discuss in a new thread if any more questions?
Regards, Garrett