AM335x Starter Kit
SDK 8.00
Looking at the following page it seems that the starter kit should default to "switch mode" when powering up:
http://processors.wiki.ti.com/index.php/SK_ETH
I've tried the following simple experiment:
- Before I started my work PC was plugged into the corporate LAN with networking operational.
- I unplugged my PC and plugged it into the Starter Kit.
- I took another network cable and plugged from the starter kit into the corporate LAN.
- I powered up the starter kit and attempted to access the network via my PC. It was not working...
Are there some other steps required to get this operational?