Hi,
We have made a custom board based on AM335x. The board bring was successful, but now we are facing an issue with Second Ethernet port. We were able to see the two Ethernet interfaces in ifconfig, the both phys are detecting and link failure is detecting in two interfaces. But we were able to ping only the first Ethernet (eth0). We were able to see the RX packets in the ifconfig for second Ethernet (eth1) is increasing, but we didn't get any ping reply from this Ethernet interface (eth1). What could be the possible reasons for this to happen.