Hi:
I am planning to do the profibus project base on AM3356, so I first run the profibus slave demo of TI on the TI's ICE V1.0 demo board. I use the profitrace as the profibus master to connect with the demo board. I set the GSD file, begin the demo code, and run wizard of ProfiTrace, profitrace has found the EVM3359 device but it is marked in yellow, which means device missed, while in manual, it is said that the device will be detect and marked with green ( device detected). I just follow the instrument of TI's wiki for profibus dp slave demo setup in AM335x. What is the problem?
Thank you very much
Best regards