Dear TI E2E Community Members,
I will design application using FPGA and external application solution (or DSP, OMAP, ARM Processor) for camera product.
The critical issue is an interface between AP and FPGA for high speed communication.
In general, it can use GPMC interface between AP and FPGA.
Could you inform about question below?
GPMC : Max bandwidth between and product name ( I known that GPMC bandwidth of IC isn't same)
If there is the speed interface higher than GMPC for interface between AP(or DSP, OMAP) and FPGA,
Could you share information such as Part number, interface name, bandwidth.
Finally,