Hi,
I am working with the AM335x starter kit and am having issues getting open communication to run the starter kit test binaries stored on the uSD card. I was able to get the correct FTDI driver installed so that they show up in the device manager but when I attempt to connect to the device using Putty (115200, same settings described in the AM335x Starter Kit ID Programming guide) I do not get anything back from the device. It is my understanding that if the device is ready for boot there should be C's printed in the terminal. I do not see any feed back when the uSD is not connected. Nor do I get any feedback when the uSD is inserted. Can you please advise as to what might be giving me issues? I have measured the clocks on the board and can verify that they are functioning correctly. What would cause the device not to initiate C's in the terminal once connected?