Hi,
I have a question about AM335x Qt.
My customer are refering to "Sitara Linux Training: Hand on with QT", and the generated HelloWorld sample application.
But when they try to execute the application on the EVM, the error message "libQt5***.so can't be found" have displayed.
The Newest Linux SDK is v01.00.00.00 and it supports Qt v5.4.
But Qt v4.8 was included to their EVM.So, it seems that libQt5***.so is not included in their EVM.
How should they do it to match Qt verision of the EVM side with the latest version?
Should I bring the all library from latest SDK? Or are there latest library released for the each EVM?
best regards,
g.f.