Hello,
I am wondering about the flexibility of the Sitara in generating clocks and PWM signals.
My first impression is that timer signals (timer4, timer5, etc.) output may work as PWM outputs once the dedicated PWM lines are full.
If this is the case, these PWM lines may hopefully be able to work as Clock signals as well.
Which peripherals would be best for generating clocks, and which would be best for PWM (after the eHRPWM and eCAP) signals?
Are the frequency of these signals configurable as well?
The highest frequency is 48MHz.
The closer the Sitara can operate like an FPGA for this application, the better.
Thanks