Hi ,
I am using AM3352BZCEA30 processor in my design, In this USB0 is terminated in the micro USB connector, We planned to use the USB in the device only mode(ID pin is flot), After Linux booting we found that the device is detected & working in the Full speed mode(12Mbs) , not switching the High speed mode(480Mbps). What could be the reason behind this scenario ? .
Pls find the other details about our hardware:
Processor used: AM3352BZCEA30
Main clock frequency:25MHz
USB interface only used in Device mode
Reagards,
Rajesh