I wanna found out if I can build a TCP/IP application base on IDK AM437x.
NDK seems suitable to my demand, however, in the description "
The code included in this NDK release is generic C code which runs on any C64P, C66,
C674, ARM9, Cortex-A8, or Cortex-M3 device. (For C6000 processors, both big-endian and little-endian
modes are supported.)
" from the introduction of NDK, AM437x(ARM Cortex-A9) is not mentioned.
That's why I am posting this question to make sure if IDK AM437x supported in this version NDK.
I would appreciate that any one give an anwser.