Hi there,
I'm attempting to debug an AM3703CUSD100 with the XDS100v2 probe in CCS 6.1. The AM3703 is failing to boot from MMC1 with SYS_BOOT[5:0] = 0b101111. I have looked at the tracing vectors and confirmed that the ROM attempted to boot from MMC1, but failed. When I try to look at one of the MMC1 registers, the value shows as "Error: unable to read". I thought that this may be because of a power domain/clock problem, but wouldn't MMC1 have to be powered and clocked as the ROM attempts to boot from it?
Possibly related - I have encountered an ST processor where I had to edit an xml file to make some registers readable by the debugger.
Any insight on the register problem (or the boot problem) would be appreciated!
Kyle