We are using customised AM335x-sk board with spi flash boot (kernel 3.14.26),
From the kernel prompt when we execute the following cmd, we are having the kernel panic.
flashcp /media/ramdisk/rootfs.jffs2 /dev/mtd7
We have created ramdisk of size 64MB and mounted on /media/ramdisk/
The kenel panic is as follows:
[ 360.712784] INFO: task jffs2_gcd_mtd6:730 blocked for more than 120 seconds.
[ 360.720197] Tainted: G W 3.14.26-ge93caaa-dirty #25
[ 360.726802] "echo 0 > /proc/sys/kernel/hung_task_timeout_secs" disables this message.
[ 360.735034] jffs2_gcd_mtd6 D c03d29f4 0 730 2 0x00000000
[ 360.741782] [<c03d29f4>] (__schedule) from [<c03d2ee8>] (schedule_preempt_disabled+0xc/0x10)
[ 360.750677] [<c03d2ee8>] (schedule_preempt_disabled) from [<c03d3cd8>] (__mutex_lock_slowpath+0x70/0xb8)
[ 360.760669] [<c03d3cd8>] (__mutex_lock_slowpath) from [<c02dacd4>] (m25p80_erase+0x58/0x318)
[ 360.769577] [<c02dacd4>] (m25p80_erase) from [<c02cbce8>] (part_erase+0x30/0x7c)
[ 360.777377] [<c02cbce8>] (part_erase) from [<c02c8abc>] (mtd_erase+0x5c/0x88)
[ 360.784910] [<c02c8abc>] (mtd_erase) from [<c019a76c>] (jffs2_erase_pending_blocks+0x318/0x664)
[ 360.794075] [<c019a76c>] (jffs2_erase_pending_blocks) from [<c0198fd4>] (jffs2_garbage_collect_pass+0x1b0/0xba0)
[ 360.804778] [<c0198fd4>] (jffs2_garbage_collect_pass) from [<c019ab5c>] (jffs2_garbage_collect_thread+0xa4/0x174)
[ 360.815579] [<c019ab5c>] (jffs2_garbage_collect_thread) from [<c004cce0>] (kthread+0xbc/0xd8)
[ 360.824569] [<c004cce0>] (kthread) from [<c000eef8>] (ret_from_fork+0x14/0x3c)
[ 360.832143] Kernel panic - not syncing: hung_task: blocked tasks
[ 360.838448] CPU: 0 PID: 391 Comm: khungtaskd Tainted: G W 3.14.26-ge93caaa-dirty #25
[ 360.847503] [<c0013f50>] (unwind_backtrace) from [<c0011588>] (show_stack+0x10/0x14)
[ 360.855652] [<c0011588>] (show_stack) from [<c03cf058>] (panic+0x7c/0x1dc)
[ 360.862891] [<c03cf058>] (panic) from [<c007f444>] (watchdog+0x284/0x2b4)
[ 360.870026] [<c007f444>] (watchdog) from [<c004cce0>] (kthread+0xbc/0xd8)
[ 360.877154] [<c004cce0>] (kthread) from [<c000eef8>] (ret_from_fork+0x14/0x3c)
Any help or input's will be appreciated
Regards,
Shrikanth